sl_bt_evt_cs_procedure_enable_complete#

Indicates the controller has scheduled a new CS procedure measurement, as a result of sl_bt_cs_procedure_enable command or disabled an ongoing, as a result of sl_bt_cs_procedure_enable command.

Modules#

sl_bt_evt_cs_procedure_enable_complete_s

Macros#

#define

Identifier of the procedure_enable_complete event.

Typedef Documentation#

sl_bt_evt_cs_procedure_enable_complete_t#

typedef struct sl_bt_evt_cs_procedure_enable_complete_s sl_bt_evt_cs_procedure_enable_complete_t

Definition at line 11953 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_cs_procedure_enable_complete_id#

#define sl_bt_evt_cs_procedure_enable_complete_id
Value:
0x025900a0

Identifier of the procedure_enable_complete event.


Definition at line 11906 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h