Data structure of the response_report event.
Public Attribute Documentation#
advertising_set#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::advertising_set
The PAwR advertising set handle
5117
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
subevent#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::subevent
The subevent that this report corresponds to
5118
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
tx_power#
int8_t sl_bt_evt_pawr_advertiser_response_report_s::tx_power
TX power value in the received packet header. Units: dBm
Range: -127 to 126
Value 127: information unavailable
5119
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
rssi#
int8_t sl_bt_evt_pawr_advertiser_response_report_s::rssi
Signal strength indicator (RSSI) of the received packet. Units: dBm
Range: -127 to +20
Value 127: information unavailable
5124
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
cte_type#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::cte_type
The CTE type
0x00: AoA CTE
0x01: AoD CTE with 1us slots
0x02: AoD CTE with 2us slots
0xFF: No CTE
5129
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
response_slot#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::response_slot
The response slot that this report corresponds to
5134
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
data_status#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::data_status
Data completeness:
0: Complete
1: Incomplete, more data to come in new events
2: Incomplete, data truncated, no more to come
255: Failed to receive subevent response in this response slot
5136
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
counter#
uint8_t sl_bt_evt_pawr_advertiser_response_report_s::counter
The sequence number of this sl_bt_evt_pawr_advertiser_response_report event as a monotonically increasing counter that wraps from 255 to 0. There is a single counter for this event type that starts from value 0 when the Bluetooth stack is started and is never reset while the stack is running. This counter can be used to detect if one or more sl_bt_evt_pawr_advertiser_response_report events have been created by the stack but dropped due to problems such as temporarily running out of resources before the event reached the application.
5144
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
data#
uint8array sl_bt_evt_pawr_advertiser_response_report_s::data
The response data that was received, if any
5158
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h