Data structure of the subevent_data_request event.

Public Attributes#

Public Attribute Documentation#

advertising_set#

uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::advertising_set

The PAwR advertising set handle


Definition at line 5057 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

subevent_start#

uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::subevent_start

The first subevent that data is requested for


Definition at line 5058 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

subevent_data_count#

uint8_t sl_bt_evt_pawr_advertiser_subevent_data_request_s::subevent_data_count

The number of subevents that data is requested for


Definition at line 5060 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h