Data structure of the report event.

Public Attributes#

uint16_t
int8_t
int8_t
uint8_t
uint8_t

Public Attribute Documentation#

sync#

uint16_t sl_bt_evt_periodic_sync_report_s::sync

Periodic advertising synchronization handle


Definition at line 4627 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

tx_power#

int8_t sl_bt_evt_periodic_sync_report_s::tx_power

TX power value in the received packet header. Units: dBm

  • Range: -127 to 126

  • Value 127: information unavailable


Definition at line 4628 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_periodic_sync_report_s::rssi

Signal strength indicator (RSSI) in the latest received packet. Units: dBm

  • Range: -127 to +20


Definition at line 4633 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

cte_type#

uint8_t sl_bt_evt_periodic_sync_report_s::cte_type

The CTE type

  • 0x00: AoA CTE

  • 0x01: AoD CTE with 1us slots

  • 0x02: AoD CTE with 2us slots

  • 0xFF: No CTE


Definition at line 4636 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

data_status#

uint8_t sl_bt_evt_periodic_sync_report_s::data_status

Data completeness:

  • 0: Complete

  • 1: Incomplete, more data to come in new events

  • 2: Incomplete, data truncated, no more to come


Definition at line 4641 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

counter#

uint8_t sl_bt_evt_periodic_sync_report_s::counter

The sequence number of this sl_bt_evt_periodic_sync_report event as a monotonically increasing counter that wraps from 255 to 0. There is a single counter for this event type that starts from value 0 when the Bluetooth stack is started and is never reset while the stack is running. This counter can be used to detect if one or more sl_bt_evt_periodic_sync_report events have been created by the stack but dropped due to problems such as temporarily running out of resources before the event reached the application.


Definition at line 4647 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_periodic_sync_report_s::data

Periodic advertising data


Definition at line 4659 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h