Data structure of the legacy_advertisement_report event.

Public Attribute Documentation#

event_flags#

uint8_t sl_bt_evt_scanner_legacy_advertisement_report_s::event_flags

The event type flag(s) in the advertisement packet. Value: One or more flags defined in Event Type Flags of Advertisement Reports


Definition at line 3352 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

address#

bd_addr sl_bt_evt_scanner_legacy_advertisement_report_s::address

Advertiser address


Definition at line 3356 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

address_type#

uint8_t sl_bt_evt_scanner_legacy_advertisement_report_s::address_type

Enum sl_bt_gap_address_type_t.

Advertiser address type.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type uses the following values:

  • 0: Public address

  • 1: Random address

If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


Definition at line 3357 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

bonding#

uint8_t sl_bt_evt_scanner_legacy_advertisement_report_s::bonding

Bonding handle if the remote advertising device has previously bonded with the local device. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle


Definition at line 3390 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_scanner_legacy_advertisement_report_s::rssi

Signal strength indicator (RSSI) in the last received packet. Units: dBm

  • Range: -127 to +20


Definition at line 3396 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

channel#

uint8_t sl_bt_evt_scanner_legacy_advertisement_report_s::channel

The channel number on which the last packet was received


Definition at line 3399 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

target_address#

bd_addr sl_bt_evt_scanner_legacy_advertisement_report_s::target_address

The target address if the advertisement is from directed advertising, otherwise ignored


Definition at line 3401 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

target_address_type#

uint8_t sl_bt_evt_scanner_legacy_advertisement_report_s::target_address_type

Enum sl_bt_gap_address_type_t.

The target address type if the advertisement is from directed advertising, otherwise ignored.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, target_address_type uses the following values:

  • 0: Public address

  • 1: Random address

If the application includes the bluetooth_feature_use_accurate_api_address_types component, target_address_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)


Definition at line 3404 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

data#

uint8array sl_bt_evt_scanner_legacy_advertisement_report_s::data

Advertising or scan response data. Ignore if this is directed advertising.


Definition at line 3440 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h