Data structure of the bonding_failed event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_sm_bonding_failed_s::connection
Connection handle
Definition at line
9974
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
reason#
uint16_t sl_bt_evt_sm_bonding_failed_s::reason
An sl_status_t code describing the error that occurred
Definition at line
9975
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h