sl_bt_evt_test_dtm_completed#

Indicates that the radio has processed a test start or end command.

The result parameter indicates the success of the command.

After the receiver or transmitter test is stopped, the number_of_packets parameter in this event indicates the number of received or transmitted packets.

Modules#

sl_bt_evt_test_dtm_completed_s

Macros#

#define

Identifier of the dtm_completed event.

Typedef Documentation#

sl_bt_evt_test_dtm_completed_t#

typedef struct sl_bt_evt_test_dtm_completed_s sl_bt_evt_test_dtm_completed_t

Definition at line 9479 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_test_dtm_completed_id#

#define sl_bt_evt_test_dtm_completed_id
Value:
0x000e00a0

Identifier of the dtm_completed event.


Definition at line 9465 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h