You are viewing documentation for version:
OTS Object Server instance type. 
Public Attributes#
sl_bt_ots_gattdb_handles_t *
GATT database handles for the Object Server Instance. 
Callbacks for the higher layers. 
uint8_t
Maximum number of concurrent connections. 
Internal database of clients. 
Public Attribute Documentation#
gattdb_handles#
sl_bt_ots_gattdb_handles_t* sl_bt_ots_server::gattdb_handles
GATT database handles for the Object Server Instance. 
callbacks#
sl_bt_ots_server_callbacks_t* sl_bt_ots_server::callbacks
Callbacks for the higher layers. 
concurrency#
uint8_t sl_bt_ots_server::concurrency
Maximum number of concurrent connections. 
features#
sl_bt_ots_features_t sl_bt_ots_server::features
Features of the server. 
client_db#
sl_bt_ots_server_client_db_entry_t* sl_bt_ots_server::client_db
Internal database of clients. 
capabilities#
sl_bt_ots_server_capabilities_t sl_bt_ots_server::capabilities
Server capabilites.