Data structure of the parameters event.
Public Attribute Documentation#
interval#
uint16_t sl_bt_evt_connection_parameters_s::interval
Connection interval. Time = Value x 1.25 ms
latency#
uint16_t sl_bt_evt_connection_parameters_s::latency
Peripheral latency (how many connection intervals the peripheral can skip)
timeout#
uint16_t sl_bt_evt_connection_parameters_s::timeout
Supervision timeout. Time = Value x 10 ms
security_mode#
uint8_t sl_bt_evt_connection_parameters_s::security_mode
Enum sl_bt_connection_security_t. Connection security mode. Values:
- sl_bt_connection_mode1_level1 (0x0): No security 
- sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption 
- sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption 
- sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key