Data structure of the remote_used_features event.
Public Attribute Documentation#
features#
uint8array sl_bt_evt_connection_remote_used_features_s::features
This parameter is 8 bytes in little endian format and contains bit fields describing the supported link layer features of the remote device. Bit value 1 means that the feature is supported.
The bits are explained in Bluetooth specification Vol 6, Part B, 4.6.