Data structure of the subrate_changed event.

Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_connection_subrate_changed_s::connection

Connection handle


subrate_factor#

uint16_t sl_bt_evt_connection_subrate_changed_s::subrate_factor

Subrate factor applied to the specified underlying connection interval.


latency#

uint16_t sl_bt_evt_connection_subrate_changed_s::latency

Peripheral latency for the connection in number of subrated connection events.


continuation_number#

uint16_t sl_bt_evt_connection_subrate_changed_s::continuation_number

Number of underlying connection events to remain active after a packet containing a Link Layer PDU with a non-zero Length field is sent or received.


timeout#

uint16_t sl_bt_evt_connection_subrate_changed_s::timeout

Supervision timeout. Time = Value x 10 ms