Data structure of the characteristic_value event.
Public Attribute Documentation#
characteristic#
uint16_t sl_bt_evt_gatt_characteristic_value_s::characteristic
GATT characteristic handle. This value is normally received from the gatt_characteristic event.
att_opcode#
uint8_t sl_bt_evt_gatt_characteristic_value_s::att_opcode
Enum sl_bt_gatt_att_opcode_t. Attribute opcode, which indicates the GATT transaction used.