Data structure of the status event.
Public Attribute Documentation#
advertising_set#
uint8_t sl_bt_evt_periodic_advertiser_status_s::advertising_set
The advertising set handle that the periodic advertising is from
status#
uint32_t sl_bt_evt_periodic_advertiser_status_s::status
The status value.
Bit 0:
0: The transmission was successful.
1: The transmission failed.
Other bits: Unused and reserved for future
event_counter#
uint16_t sl_bt_evt_periodic_advertiser_status_s::event_counter
The event counter of the transmission