GATT Attribute State Flags#

Defines the attribute state flags for GATT attributes.

Macros#

#define

The attribute is visible to remote GATT clients.

#define

The attribute has been marked to be activated when the changes are committed.

#define

The attribute has been marked to be inactivated when the changes are committed.

#define

The attribute has been marked to be added when the changes are committed.

#define

The attribute has been marked to be deleted when the changes are committed.

Macro Definition Documentation#

SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ACTIVE#

#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ACTIVE
Value:
0x1

The attribute is visible to remote GATT clients.


SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STARTED#

#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STARTED
Value:
0x2

The attribute has been marked to be activated when the changes are committed.


SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STOPPED#

#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STOPPED
Value:
0x4

The attribute has been marked to be inactivated when the changes are committed.


SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ADDED#

#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ADDED
Value:
0x8

The attribute has been marked to be added when the changes are committed.


SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_DELETED#

#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_DELETED
Value:
0x10

The attribute has been marked to be deleted when the changes are committed.