Security Manager configuration flags#
These values are used to configure security requirements.
Macros#
#define
SL_BT_SM_CONFIGURATION_MITM_REQUIRED 0x1
Bonding requires authentication (Man-in-the-Middle protection).
#define
SL_BT_SM_CONFIGURATION_BONDING_REQUIRED 0x2
Encryption requires bonding. Note that this setting will also enable bonding.
#define
SL_BT_SM_CONFIGURATION_SC_ONLY 0x4
Require secure connections pairing.
#define
SL_BT_SM_CONFIGURATION_BONDING_REQUEST_REQUIRED 0x8
Bonding requests need to be confirmed. Received bonding requests are notified by sl_bt_evt_sm_confirm_bonding.
#define
SL_BT_SM_CONFIGURATION_CONNECTIONS_FROM_BONDED_DEVICES_ONLY 0x10
Allow connections only from bonded devices. This option is ignored when the application includes the bluetooth_feature_external_bonding_database feature.
#define
SL_BT_SM_CONFIGURATION_PREFER_MITM 0x20
Prefer authenticated pairing when both options are possible based on the settings. Otherwise just works pairing is preferred.
#define
SL_BT_SM_CONFIGURATION_OOB_FROM_BOTH_DEVICES_REQUIRED 0x40
Require secure connections OOB data from both devices.
#define
SL_BT_SM_CONFIGURATION_REJECT_DEBUG_KEYS 0x80
Reject pairing if remote device uses debug keys.