Data structure containing high-level results along with CS procedure data and ranging data in a serialized and fragmented format.

The content elements placed in the following order:

  • result size (1 byte)

  • result buffer content (variable size; type is 1 byte, value is typically 4 bytes)

  • number of steps (1 byte)

  • step channel array (variable size, 1 byte per step)

  • initiator ranging data size (4 bytes)

  • initiator RAS data (variable size)

  • reflector ranging data size (4 bytes)

  • reflector RAS data (variable size)

This entire data content will be fragmented and sent to the host application

Public Attributes#

uint8_t

Number of fragments left.

uint8array

Content of the fragment.

Public Attribute Documentation#

fragments_left#

uint8_t cs_acp_extended_result_evt_t::fragments_left

Number of fragments left.


fragment#

uint8array cs_acp_extended_result_evt_t::fragment

Content of the fragment.