Data structure that contains the necessary details about the actual configuration of the target device.

Public Attributes#

uint8_t

Target config bitfield.

uint8_t

Maximum initiator instance count.

uint8_t

Maximum BLE connections.

Public Attribute Documentation#

target_config_bitfield#

uint8_t cs_acp_get_target_config_rsp_t::target_config_bitfield

Target config bitfield.


max_initiator_instance_count#

uint8_t cs_acp_get_target_config_rsp_t::max_initiator_instance_count

Maximum initiator instance count.


max_bluetooth_connections#

uint8_t cs_acp_get_target_config_rsp_t::max_bluetooth_connections

Maximum BLE connections.