sl_bt_evt_advertiser_scan_request#

Reports a scan request received during the legacy or extended advertising advertising if the scan request notification is enabled.

Modules#

sl_bt_evt_advertiser_scan_request_s

Macros#

#define

Identifier of the scan_request event.

Typedef Documentation#

sl_bt_evt_advertiser_scan_request_t#

typedef struct sl_bt_evt_advertiser_scan_request_s sl_bt_evt_advertiser_scan_request_t

Definition at line 2360 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_advertiser_scan_request_id#

#define sl_bt_evt_advertiser_scan_request_id
Value:
0x020400a0

Identifier of the scan_request event.


Definition at line 2313 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h