Data structure of the completed event.
Public Attribute Documentation#
analyzer#
uint8_t sl_bt_evt_connection_analyzer_completed_s::analyzer
The handle of the connection analyzer
Definition at line
14590
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
reason#
uint16_t sl_bt_evt_connection_analyzer_completed_s::reason
An sl_status_t code describing the reason of stopping the operation
Definition at line
14591
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h