You are viewing documentation for version:
9.0.0 (latest)
sl_bt_evt_gatt_descriptor#
Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.
It is generated after issuing the sl_bt_gatt_discover_descriptors or sl_bt_gatt_discover_characteristic_descriptors command.
Modules#
sl_bt_evt_gatt_descriptor_s
Macros#
#define
Identifier of the descriptor event.
Typedef Documentation#
sl_bt_evt_gatt_descriptor_t#
typedef struct sl_bt_evt_gatt_descriptor_s sl_bt_evt_gatt_descriptor_t
Definition at line 7693
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_gatt_descriptor_id#
#define sl_bt_evt_gatt_descriptor_id
Value:0x030900a0
Identifier of the descriptor event.
Definition at line 7681
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h