sl_bt_evt_system_stopped#

When the Bluetooth on-demand start component is included in the application build, this event is triggered when stopping the Bluetooth stack using commands sl_bt_system_stop_bluetooth or sl_bt_system_forcefully_stop_bluetooth has completed.

Macros#

#define

Identifier of the stopped event.

Macro Definition Documentation#

sl_bt_evt_system_stopped_id#

#define sl_bt_evt_system_stopped_id
Value:
0x010100a0

Identifier of the stopped event.


Definition at line 802 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h