Data structure of the dtm_completed event.
Public Attribute Documentation#
result#
uint16_t sl_bt_evt_test_dtm_completed_s::result
Command result
Definition at line
9501
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
number_of_packets#
uint16_t sl_bt_evt_test_dtm_completed_s::number_of_packets
Number of packets
Only valid for sl_bt_test_dtm_end command.
Definition at line
9502
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h