GATT Attribute State Flags#
Defines the attribute state flags for GATT attributes.
Macro Definition Documentation#
SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ACTIVE#
#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ACTIVEValue:
0x1
The attribute is visible to remote GATT clients.
Definition at line
8682
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STARTED#
#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STARTEDValue:
0x2
The attribute has been marked to be activated when the changes are committed.
Definition at line
8686
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STOPPED#
#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_STOPPEDValue:
0x4
The attribute has been marked to be inactivated when the changes are committed.
Definition at line
8690
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ADDED#
#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_ADDEDValue:
0x8
The attribute has been marked to be added when the changes are committed.
Definition at line
8693
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_DELETED#
#define SL_BT_GATTDB_ATTRIBUTE_STATE_FLAG_DELETEDValue:
0x10
The attribute has been marked to be deleted when the changes are committed.
Definition at line
8697
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h