Task specific data of list application keys bound to model.
Public Attributes#
uint8_t
Index of the element where the model resides on the node.
uint16_t
Vendor ID for the model (0xFFFF for Bluetooth SIG models)
uint16_t
Model ID for the model.
uint16_t *
List of key indexes for the application keys which are bound to a model.
uint16_t
Number of key indexes for the application keys which are bound to a model.
Public Attribute Documentation#
elem_index#
uint8_t btmesh_conf_task_model_bindings_list_t::elem_index
Index of the element where the model resides on the node.
vendor_id#
uint16_t btmesh_conf_task_model_bindings_list_t::vendor_id
Vendor ID for the model (0xFFFF for Bluetooth SIG models)
appkey_indexes#
uint16_t* btmesh_conf_task_model_bindings_list_t::appkey_indexes
List of key indexes for the application keys which are bound to a model.
appkey_count#
uint16_t btmesh_conf_task_model_bindings_list_t::appkey_count
Number of key indexes for the application keys which are bound to a model.