Task specific data of set/get relay feature.

Public Attributes#

uint8_t

Relay value. Valid values are:

uint8_t

Relay retransmit count. Valid values range from 0 to 7; default value is 0 (no retransmissions).

uint16_t

Relay retransmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the retransmission count is set to zero.

Public Attribute Documentation#

value#

uint8_t btmesh_conf_task_relay_t::value

Relay value. Valid values are:

  • 0: Relay feature is disabled

  • 1: Relay feature is enabled


retransmit_count#

uint8_t btmesh_conf_task_relay_t::retransmit_count

Relay retransmit count. Valid values range from 0 to 7; default value is 0 (no retransmissions).


retransmit_interval_ms#

uint16_t btmesh_conf_task_relay_t::retransmit_interval_ms

Relay retransmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the retransmission count is set to zero.