Task specific data of set/get network transmit count and interval.

Public Attributes#

uint8_t

Network transmit count. Valid values range from 1 to 8; default value is 1 (single transmission; no retransmissions).

uint16_t

Network transmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the transmission count is set to one.

Public Attribute Documentation#

transmit_count#

uint8_t btmesh_conf_task_network_transmit_t::transmit_count

Network transmit count. Valid values range from 1 to 8; default value is 1 (single transmission; no retransmissions).


transmit_interval_ms#

uint16_t btmesh_conf_task_network_transmit_t::transmit_interval_ms

Network transmit interval in milliseconds. Valid values range from 10 ms to 320 ms, with a resolution of 10 ms. The value is ignored if the transmission count is set to one.