Bluetooth Mesh Scene Setup Server Model#

Bluetooth Mesh Scene Setup Server Model.

Bluetooth Mesh Scene model Setup Server functionality.

Modules#

sl_btmesh_evt_scene_setup_server_store

sl_btmesh_evt_scene_setup_server_delete

sl_btmesh_evt_scene_setup_server_publish

Functions#

sl_status_t

Macros#

#define
sl_btmesh_cmd_scene_setup_server_init_id 0x00510028
#define
sl_btmesh_rsp_scene_setup_server_init_id 0x00510028

Function Documentation#

sl_btmesh_scene_setup_server_init#

sl_status_t sl_btmesh_scene_setup_server_init (uint16_t elem_index)
Parameters
TypeDirectionArgument NameDescription
uint16_t[in]elem_index

Index of the element.

Initialize the Scene Setup Server model. Server does not have any internal configurations. The command only activates the model in the mesh stack.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.