sl_btmesh_evt_mbt_client_transfer_complete#
The transfer is complete.
This event indicates that the transfer is complete, either successfully or unsuccessfully. Servers which have failed before the transfer is complete, indicated by sl_btmesh_evt_mbt_client_server_failed event, have failed to receive the full object. All other servers have received the full object successfully. The sl_btmesh_mbt_client_get_status command may be used to get the current status of each server to determine if the transfer to a specific server succeeded or not. Servers which successfully completed the transfer are marked with status done.
Modules#
sl_btmesh_evt_mbt_client_transfer_complete_s
Typedefs#
Macros#
#define
Identifier of the transfer_complete event.