Power consumption mock sensor#
The power consumption mock sensor is an application-level software module that simulates power consumption measurements. This module provides interface for setting and getting the simulated power consumption. This component is prepared for integration into SOC applications. This is a No-Code component, if it is used with Sensor Server to broadcast power consumption data to sensor clients.
Function Documentation#
sl_btmesh_set_power_consumption#
void sl_btmesh_set_power_consumption (energy32_t energy_usage)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| energy32_t | [in] | energy_usage | Power consumption value to set  | 
Set the power consumption value. It could be used to initialize the sensor.
sl_btmesh_get_power_consumption#
energy32_t sl_btmesh_get_power_consumption (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Get the current power consumption value measured by sensor.
Returns
Current value of power consumption.