NCP User Commands#
Demonstrates the communication between an NCP host and NCP target using BGAPI user messages, responses and events. Can be used as a starting point for creating custom commands or for testing purposes.
Functions#
void
sl_ncp_app_user_cmd_message_to_target_cb(void *data)
void
ncp_cmd_to_target_handler(void *data, bool *cmd_handled)
Function Documentation#
sl_ncp_app_user_cmd_message_to_target_cb#
void sl_ncp_app_user_cmd_message_to_target_cb (void * data)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void * | [in] | data | Data received from NCP through UART.  | 
Application user command (message_to_target) handler callback.
Handle user defined commands received from NCP-host in application.
ncp_cmd_to_target_handler#
void ncp_cmd_to_target_handler (void * data, bool * cmd_handled)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void * | [in] | data | Pointer to the data received from NCP host  | 
| bool * | [out] | cmd_handled | Flag to indicate if the command is handled  | 
This function handles user defined commands received from NCP host.