NCP DFU Utility#
Implements the Firmware Update Information Status message assembly, with provided interfaces for setting FWIDs and URIs with indexing. This component is prepared for integration into NCP applications.
Functions#
Function Documentation#
sl_btmesh_ncp_dfu_set_fwid#
sl_status_t sl_btmesh_ncp_dfu_set_fwid (uint8_t idx, uint8_t len, uint8_t * data)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | idx | Index of the FW |
| uint8_t | [in] | len | Length of the data |
| uint8_t * | [in] | data | Firmware ID data; containing CID and version information |
Sets the Firmware ID for the given index, as part of the FW information
Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_INVALID_PARAMETER: If length is less than 2 or greater than 108
SL_STATUS_NO_MORE_RESOURCE: In case memory allocation error
sl_btmesh_ncp_dfu_set_uri#
sl_status_t sl_btmesh_ncp_dfu_set_uri (uint8_t idx, uint8_t type, uint8_t len, uint8_t * data)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | idx | Index of the FW |
| uint8_t | [in] | type | Type of the command; '0' erases and writes new URI, '1' appends to existing URI. |
| uint8_t | [in] | len | Length of the data |
| uint8_t * | [in] | data | The data to write or append |
Sets the URI for given index, as part of the FW information
Returns
Status code
Return values
SL_STATUS_OK: In case of success
SL_STATUS_NO_MORE_RESOURCE: In case of memory allocation error
SL_STATUS_INVALID_PARAMETER: In case the combined length of the URI is longer than 255 bytes
sl_btmesh_ncp_dfu_handle_cmd#
void sl_btmesh_ncp_dfu_handle_cmd (void * data, bool * cmd_handled)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | data | Pointer to the command. |
| bool * | [inout] | cmd_handled | Status of the command: true - cmd handled, no further interpretation is required false - cmd unhandled, interpretation is required |
User command (message_to_target) handler callback. Handles user defined commands received from NCP host.
Note
If the value of the parameter 'cmd_handled' is false, the incoming command needs to be interpreted. If the command is recognized and handled, the 'cmd_handled' flag should be set to true. If the value of the 'cmd_handled' parameter is already true, the function will return without executing any further operations.