EmberCommandEntry Struct Reference
Command entry for a command table. More...
#include <
command-interpreter2.h
>
Data Fields |
|
PGM_P | name |
CommandAction | action |
PGM_P | argumentTypes |
PGM_P | description |
Command entry for a command table.
Definition at line
142
of file
command-interpreter2.h
.
Field Documentation
CommandAction EmberCommandEntry::action |
A reference to a function in the application that implements the command. If this entry refers to a nested command, the action field has to be set to NULL.
Definition at line
161
of file
command-interpreter2.h
.
PGM_P EmberCommandEntry::argumentTypes |
For normal, non-nested, commands, argumentTypes is a string that specifies the number and types of arguments the command accepts. The argument specifiers are:
- u: one-byte unsigned integer.
- v: two-byte unsigned integer
- w: four-byte unsigned integer
- s: one-byte signed integer
- b: string. The argument can be entered in ASCII by using quotes, for example: "foo". It can also be entered in hexadecimal values by using curly braces, for example: { 08 A1 f2 }. The number of hexadecimal digits must be even and spaces are ignored.
- *: zero or more of the previous type. If used, this must be the last specifier.
- ?: unknown number of arguments. If used this must be the only character, which means that the command interpreter will not perform any validation of arguments and will call the action directly trusting that it will handle whatever arguments are passed in. Integer arguments can be either decimal or hexadecimal. A 0x prefix indicates a hexadecimal integer, for example: 0x3ed.
For a nested command (action is NULL), argumentTypes will contain a pointer to the nested commands.
Definition at line
190
of file
command-interpreter2.h
.
PGM_P EmberCommandEntry::description |
A description of the command.
Definition at line
195
of file
command-interpreter2.h
.
PGM_P EmberCommandEntry::name |
Use letters, digits, and underscores, '_', for the command name. Command names are case-sensitive.
Definition at line
149
of file
command-interpreter2.h
.
The documentation for this struct was generated from the following file:
-
command-interpreter2.h