EmberOutgoingMacMessage Struct Reference
An instance of this structure is passed to emberMacMessageSentHandler() . It describes the outgoing MAC frame. More...
#include <
ember-types.h
>
Data Fields |
|
| EmberMessageOptions | options |
| EmberMacFrame | macFrame |
| uint8_t | tag |
| uint32_t | frameCounter |
| EmberMessageLength | length |
| uint8_t * | payload |
| int8_t | ackRssi |
An instance of this structure is passed to emberMacMessageSentHandler() . It describes the outgoing MAC frame.
Definition at line
387
of file
ember-types.h
.
Field Documentation
| int8_t EmberOutgoingMacMessage::ackRssi |
The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.
Definition at line
421
of file
ember-types.h
.
| uint32_t EmberOutgoingMacMessage::frameCounter |
The security frame counter of the outgoing MAC frame (if any).
Definition at line
406
of file
ember-types.h
.
| EmberMessageLength EmberOutgoingMacMessage::length |
An EmberMessageLength value indicating the length in bytes of the incoming message.
Definition at line
411
of file
ember-types.h
.
| EmberMacFrame EmberOutgoingMacMessage::macFrame |
An EmberMacFrame struct indicating the source and destination addresses and source and destination PAN IDs of the outgoing MAC frame.
Definition at line
397
of file
ember-types.h
.
| EmberMessageOptions EmberOutgoingMacMessage::options |
An EmberMessageOptions value indicating the options used for transmitting the outgoing message.
Definition at line
392
of file
ember-types.h
.
| uint8_t* EmberOutgoingMacMessage::payload |
A pointer to the message payload.
Definition at line
415
of file
ember-types.h
.
| uint8_t EmberOutgoingMacMessage::tag |
A tag value the application can use to match emberMacMessageSend() calls to the corresponding emberMacMessageSentHandler() calls.
Definition at line
402
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h