EmberCommandState Struct Reference
For use when declaring a separate command streams. The fields are not accessed directly by the application. More...
#include <
command-interpreter2.h
>
Data Fields |
|
| uint8_t | state |
| uint8_t | buffer [ EMBER_COMMAND_BUFFER_LENGTH ] |
| uint8_t | tokenIndices [ MAX_TOKEN_COUNT +1] |
| uint8_t | tokenCount |
| uint16_t | index |
| uint8_t | error |
| uint8_t | hexHighNibble |
| uint8_t | argOffset |
| uint8_t | previousCharacter |
| uint8_t | defaultBase |
| EmberCommandEntry * | currentCommand |
For use when declaring a separate command streams. The fields are not accessed directly by the application.
Definition at line
406
of file
command-interpreter2.h
.
Field Documentation
| uint8_t EmberCommandState::argOffset |
Definition at line
432
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::buffer[ EMBER_COMMAND_BUFFER_LENGTH ] |
Definition at line
413
of file
command-interpreter2.h
.
| EmberCommandEntry * EmberCommandState::currentCommand |
Definition at line
442
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::defaultBase |
Definition at line
439
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::error |
Definition at line
426
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::hexHighNibble |
Definition at line
429
of file
command-interpreter2.h
.
| uint16_t EmberCommandState::index |
Definition at line
423
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::previousCharacter |
Definition at line
436
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::state |
Definition at line
408
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::tokenCount |
Definition at line
420
of file
command-interpreter2.h
.
| uint8_t EmberCommandState::tokenIndices[ MAX_TOKEN_COUNT +1] |
Definition at line
417
of file
command-interpreter2.h
.
The documentation for this struct was generated from the following file:
-
command-interpreter2.h