An instance of this structure is passed to emberMacMessageSentHandler(). It describes the outgoing MAC frame.

Public Attribute Documentation#

options#

EmberMessageOptions EmberOutgoingMacMessage::options

An EmberMessageOptions value indicating the options used for transmitting the outgoing message.


macFrame#

EmberMacFrame EmberOutgoingMacMessage::macFrame

An EmberMacFrame struct indicating the source and destination addresses and source and destination PAN IDs of the outgoing MAC frame.


tag#

uint8_t EmberOutgoingMacMessage::tag

A tag value the application can use to match emberMacMessageSend() calls to the corresponding emberMacMessageSentHandler() calls.


frameCounter#

uint32_t EmberOutgoingMacMessage::frameCounter

The security frame counter of the outgoing MAC frame (if any).


length#

EmberMessageLength EmberOutgoingMacMessage::length

An EmberMessageLength value indicating the length in bytes of the incoming message.


payload#

uint8_t* EmberOutgoingMacMessage::payload

A pointer to the message payload.


ackRssi#

int8_t EmberOutgoingMacMessage::ackRssi

The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.


timestamp#

uint32_t EmberOutgoingMacMessage::timestamp

The millisecond system time returned by halCommonGetInt32uMillisecondTick() at the time the sync word was transmitted.