The static part of an event. Each event can be used with only one event queue.

Public Attributes#

void(*
void(*
const char *

Public Attribute Documentation#

queue#

struct EventQueue_s* EventActions::queue

Definition at line 550 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/ember-types.h

handler#

void(* EventActions::handler) (struct Event_s *)

Definition at line 551 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/ember-types.h

marker#

void(* EventActions::marker) (struct Event_s *)

Definition at line 552 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/ember-types.h

name#

const char* EventActions::name

Definition at line 553 of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/ember-types.h