A structure that stores an 802.15.4 address.
Public Attributes#
uint8_t
Long (EUI-64) address. Valid if mode is EMBER_MAC_ADDRESS_MODE_LONG.
uint16_t
Short address (node ID). Valid if mode is EMBER_MAC_ADDRESS_MODE_SHORT.
union EmberMacAddress::@3
Public Attribute Documentation#
longAddress#
uint8_t EmberMacAddress::longAddress[EUI64_SIZE]
Long (EUI-64) address. Valid if mode is EMBER_MAC_ADDRESS_MODE_LONG.
shortAddress#
uint16_t EmberMacAddress::shortAddress
Short address (node ID). Valid if mode is EMBER_MAC_ADDRESS_MODE_SHORT.