An instance of this structure is passed to emberMessageSentHandler(). It describes the outgoing packet.
Public Attribute Documentation#
options#
EmberMessageOptions EmberOutgoingMessage::options
An EmberMessageOptions value indicating the options used for transmitting the outgoing message.
298
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
destination#
EmberNodeId EmberOutgoingMessage::destination
An EmberNodeId value indicating the destination short ID.
302
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
endpoint#
uint8_t EmberOutgoingMessage::endpoint
The endpoint the message is destined to.
306
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
tag#
uint8_t EmberOutgoingMessage::tag
A tag value the application can use to match emberMessageSend() calls to the corresponding emberMessageSentHandler() calls.
311
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
length#
EmberMessageLength EmberOutgoingMessage::length
An EmberMessageLength value indicating the length in bytes of the incoming message.
316
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
payload#
uint8_t* EmberOutgoingMessage::payload
A pointer to the message payload.
320
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
ackRssi#
int8_t EmberOutgoingMessage::ackRssi
The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.
326
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h
timestamp#
uint32_t EmberOutgoingMessage::timestamp
The millisecond system time returned by ::sl_sleeptimer at the time the sync word was transmitted.
331
of file /mnt/raid/workspaces/ws.04isO4uyE/overlay/gsdk/protocol/flex/stack/include/ember-types.h