Single conversion initialization structure.
Public Attributes#
Peripheral reflex system trigger selection.
Acquisition time (in ADC clock cycles).
Sample reference selection.
Sample resolution.
Sample input selection, use single-ended or differential input according to setting of diff
.
Select if single-ended or differential input.
Peripheral reflex system trigger enable.
Select if left adjustment should be done.
Select if continuous conversion until explicit stop.
Public Attribute Documentation#
prsSel#
ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel
Peripheral reflex system trigger selection.
Only applicable if prsEnable
is enabled.
967
of file platform/emlib/inc/em_adc.h
acqTime#
ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime
Acquisition time (in ADC clock cycles).
970
of file platform/emlib/inc/em_adc.h
reference#
ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference
Sample reference selection.
Note that, for external references, the ADC calibration register must be set explicitly.
976
of file platform/emlib/inc/em_adc.h
resolution#
ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution
Sample resolution.
979
of file platform/emlib/inc/em_adc.h
input#
ADC_SingleInput_TypeDef ADC_InitSingle_TypeDef::input
Sample input selection, use single-ended or differential input according to setting of diff
.
986
of file platform/emlib/inc/em_adc.h
diff#
bool ADC_InitSingle_TypeDef::diff
Select if single-ended or differential input.
1001
of file platform/emlib/inc/em_adc.h
prsEnable#
bool ADC_InitSingle_TypeDef::prsEnable
Peripheral reflex system trigger enable.
1004
of file platform/emlib/inc/em_adc.h
leftAdjust#
bool ADC_InitSingle_TypeDef::leftAdjust
Select if left adjustment should be done.
1007
of file platform/emlib/inc/em_adc.h
rep#
bool ADC_InitSingle_TypeDef::rep
Select if continuous conversion until explicit stop.
1010
of file platform/emlib/inc/em_adc.h