HFXO initialization structure.
Initialization values should be obtained from a configuration tool, application note or crystal data sheet.
Public Attributes#
uint8_t
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.
uint8_t
Startup delay.
bool
Enable/disable glitch detector.
Oscillator mode.
Public Attribute Documentation#
boost#
uint8_t CMU_HFXOInit_TypeDef::boost
HFXO Boost, 0=50% 1=70%, 2=80%, 3=100%.
Definition at line
3172
of file platform/emlib/inc/em_cmu.h
timeout#
uint8_t CMU_HFXOInit_TypeDef::timeout
Startup delay.
Definition at line
3173
of file platform/emlib/inc/em_cmu.h
glitchDetector#
bool CMU_HFXOInit_TypeDef::glitchDetector
Enable/disable glitch detector.
Definition at line
3174
of file platform/emlib/inc/em_cmu.h
mode#
CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode
Oscillator mode.
Definition at line
3176
of file platform/emlib/inc/em_cmu.h