Callback structure that can be used to define DMA complete actions.
A reference to this structure is only stored in the primary descriptor for a channel (if using callback feature). If callback is required for both primary and alternate descriptor completion, this must be handled by one common callback, using the provided 'primary' parameter with the callback function.
Public Attributes#
Pointer to callback function to invoke when DMA transfer cycle is done.
User defined pointer to provide with callback function.
For internal use only: Indicates if next callback applies to primary or alternate descriptor completion.
Public Attribute Documentation#
cbFunc#
DMA_FuncPtr_TypeDef DMA_CB_TypeDef::cbFunc
Pointer to callback function to invoke when DMA transfer cycle is done.
Notice that this function is invoked in interrupt context, and therefore should be short and non-blocking.
138
of file platform/emlib/inc/em_dma.h
userPtr#
void* DMA_CB_TypeDef::userPtr
User defined pointer to provide with callback function.
141
of file platform/emlib/inc/em_dma.h
primary#
uint8_t DMA_CB_TypeDef::primary
For internal use only: Indicates if next callback applies to primary or alternate descriptor completion.
Mainly useful for ping-pong DMA cycles. Set this value to 0 prior to configuring callback handling.
148
of file platform/emlib/inc/em_dma.h