Code execution configuration.
Public Attributes#
bool
Enable Suppressed Conditional Branch Target Prefetch.
bool
Enable MSC prefetching.
bool
Disable instruction cache.
bool
Disable automatic cache invalidation on write or erase.
bool
Disable automatic caching of fetches in interrupt context.
bool
Use ahb_hprot to determine if the instruction is cacheable or not.
Public Attribute Documentation#
scbtEn#
bool MSC_ExecConfig_TypeDef::scbtEn
Enable Suppressed Conditional Branch Target Prefetch.
Definition at line
230
of file platform/emlib/inc/em_msc.h
prefetchEn#
bool MSC_ExecConfig_TypeDef::prefetchEn
Enable MSC prefetching.
Definition at line
231
of file platform/emlib/inc/em_msc.h
ifcDis#
bool MSC_ExecConfig_TypeDef::ifcDis
Disable instruction cache.
Definition at line
232
of file platform/emlib/inc/em_msc.h
aiDis#
bool MSC_ExecConfig_TypeDef::aiDis
Disable automatic cache invalidation on write or erase.
Definition at line
233
of file platform/emlib/inc/em_msc.h
iccDis#
bool MSC_ExecConfig_TypeDef::iccDis
Disable automatic caching of fetches in interrupt context.
Definition at line
234
of file platform/emlib/inc/em_msc.h
useHprot#
bool MSC_ExecConfig_TypeDef::useHprot
Use ahb_hprot to determine if the instruction is cacheable or not.
Definition at line
235
of file platform/emlib/inc/em_msc.h