SE status.
Public Attributes#
uint32_t
Boot status code / error code (Bits [7:0]).
uint32_t
SE firmware version.
uint32_t
Host firmware version (if available).
Debug lock status.
bool
Secure boot enabled.
Public Attribute Documentation#
bootStatus#
uint32_t SE_Status_t::bootStatus
Boot status code / error code (Bits [7:0]).
Definition at line
570
of file platform/emlib/inc/em_se.h
seFwVersion#
uint32_t SE_Status_t::seFwVersion
SE firmware version.
Definition at line
572
of file platform/emlib/inc/em_se.h
hostFwVersion#
uint32_t SE_Status_t::hostFwVersion
Host firmware version (if available).
Definition at line
574
of file platform/emlib/inc/em_se.h
debugStatus#
SE_DebugStatus_t SE_Status_t::debugStatus
Debug lock status.
Definition at line
576
of file platform/emlib/inc/em_se.h
secureBootEnabled#
bool SE_Status_t::secureBootEnabled
Secure boot enabled.
Definition at line
578
of file platform/emlib/inc/em_se.h