TCP/IP communication module#
The TCP/IP communication module provides for a channel of communication for the SSL/TLS communication module to use.
In the TCP/IP-model it provides for communication up to the Transport (or Host-to-host) layer. SSL/TLS resides on top of that, in the Application layer, and makes use of its basic provisions:
listening on a port (see
mbedtls_net_bind()
).accepting a connection (through
mbedtls_net_accept()
).read/write (through
mbedtls_net_recv()/mbedtls_net_send())
.close a connection (through
mbedtls_net_close()
).
This way you have the means to, for example, implement and use an UDP or IPSec communication solution as a basis.
This module can be used at server- and clientside to provide a basic means of communication over the internet.