Secure Element Message Authentication Codes#
Generation and authentication of Message Authentication Codes (MACs) using a secure element can be done either as a single function call (via the psa_drv_se_mac_generate_t
or psa_drv_se_mac_verify_t
functions), or in parts using the following sequence:
psa_drv_se_mac_setup_t
psa_drv_se_mac_update_t
psa_drv_se_mac_update_t
...
psa_drv_se_mac_finish_t
orpsa_drv_se_mac_finish_verify_t
If a previously started secure element MAC operation needs to be terminated, it should be done so by the psa_drv_se_mac_abort_t
. Failure to do so may result in allocated resources not being freed or in other undefined behavior.
Modules#
Typedefs#
A function that starts a secure element MAC operation for a PSA Crypto Driver implementation.
A function that continues a previously started secure element MAC operation.
a function that completes a previously started secure element MAC operation by returning the resulting MAC.
A function that completes a previously started secure element MAC operation by comparing the resulting MAC against a provided value.
A function that aborts a previous started secure element MAC operation.
A function that performs a secure element MAC operation in one command and returns the calculated MAC.
A function that performs a secure element MAC operation in one command and compares the resulting MAC against a provided value.
Typedef Documentation#
psa_drv_se_mac_setup_t#
typedef psa_status_t(* psa_drv_se_mac_setup_t) (psa_drv_se_context_t *drv_context, void *op_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm) )(psa_drv_se_context_t *drv_context, void *op_context, psa_key_slot_number_t key_slot, psa_algorithm_t algorithm)
A function that starts a secure element MAC operation for a PSA Crypto Driver implementation.
[inout] | drv_context | The driver context structure. |
[inout] | op_context | A structure that will contain the hardware-specific MAC context |
[in] | key_slot | The slot of the key to be used for the operation |
[in] | algorithm | The algorithm to be used to underly the MAC operation |
185
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_update_t#
typedef psa_status_t(* psa_drv_se_mac_update_t) (void *op_context, const uint8_t *p_input, size_t input_length) )(void *op_context, const uint8_t *p_input, size_t input_length)
A function that continues a previously started secure element MAC operation.
[inout] | op_context | A hardware-specific structure for the previously-established MAC operation to be updated |
[in] | p_input | A buffer containing the message to be appended to the MAC operation |
[in] | input_length | The size in bytes of the input message buffer |
200
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_finish_t#
typedef psa_status_t(* psa_drv_se_mac_finish_t) (void *op_context, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) )(void *op_context, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length)
a function that completes a previously started secure element MAC operation by returning the resulting MAC.
[inout] | op_context | A hardware-specific structure for the previously started MAC operation to be finished |
[out] | p_mac | A buffer where the generated MAC will be placed |
[in] | mac_size | The size in bytes of the buffer that has been allocated for the |
[out] | p_mac_length | After completion, will contain the number of bytes placed in the |
220
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_finish_verify_t#
typedef psa_status_t(* psa_drv_se_mac_finish_verify_t) (void *op_context, const uint8_t *p_mac, size_t mac_length) )(void *op_context, const uint8_t *p_mac, size_t mac_length)
A function that completes a previously started secure element MAC operation by comparing the resulting MAC against a provided value.
[inout] | op_context | A hardware-specific structure for the previously started MAC operation to be fiinished |
[in] | p_mac | The MAC value against which the resulting MAC will be compared against |
[in] | mac_length | The size in bytes of the value stored in |
241
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_abort_t#
typedef psa_status_t(* psa_drv_se_mac_abort_t) (void *op_context) )(void *op_context)
A function that aborts a previous started secure element MAC operation.
[inout] | op_context | A hardware-specific structure for the previously started MAC operation to be aborted |
251
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_generate_t#
typedef psa_status_t(* psa_drv_se_mac_generate_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length) )(psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, uint8_t *p_mac, size_t mac_size, size_t *p_mac_length)
A function that performs a secure element MAC operation in one command and returns the calculated MAC.
[inout] | drv_context | The driver context structure. |
[in] | p_input | A buffer containing the message to be MACed |
[in] | input_length | The size in bytes of |
[in] | key_slot | The slot of the key to be used |
[in] | alg | The algorithm to be used to underlie the MAC operation |
[out] | p_mac | A buffer where the generated MAC will be placed |
[in] | mac_size | The size in bytes of the |
[out] | p_mac_length | After completion, will contain the number of bytes placed in the |
271
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h
psa_drv_se_mac_verify_t#
typedef psa_status_t(* psa_drv_se_mac_verify_t) (psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, const uint8_t *p_mac, size_t mac_length) )(psa_drv_se_context_t *drv_context, const uint8_t *p_input, size_t input_length, psa_key_slot_number_t key_slot, psa_algorithm_t alg, const uint8_t *p_mac, size_t mac_length)
A function that performs a secure element MAC operation in one command and compares the resulting MAC against a provided value.
[inout] | drv_context | The driver context structure. |
[in] | p_input | A buffer containing the message to be MACed |
[in] | input_length | The size in bytes of |
[in] | key_slot | The slot of the key to be used |
[in] | alg | The algorithm to be used to underlie the MAC operation |
[in] | p_mac | The MAC value against which the resulting MAC will be compared against |
[in] | mac_length | The size in bytes of |
300
of file util/third_party/mbedtls/include/psa/crypto_se_driver.h