Password-authenticated key exchange (PAKE)#
This is a proposed PAKE interface for the PSA Crypto API.
It is not part of the official PSA Crypto API yet.
Note
The content of this section is not part of the stable API and ABI of Mbed Crypto and may change arbitrarily from version to version. Same holds for the corresponding macros #PSA_ALG_CATEGORY_PAKE and PSA_ALG_JPAKE.
Typedefs#
Encoding of the application role of PAKE.
Encoding of input and output indicators for PAKE.
Encoding of the type of the PAKE's primitive.
Encoding of the family of the primitive associated with the PAKE.
Encoding of the primitive associated with the PAKE.
Functions#
Return an initial value for a PAKE cipher suite object.
Retrieve the PAKE algorithm from a PAKE cipher suite.
Declare the PAKE algorithm for the cipher suite.
Retrieve the primitive from a PAKE cipher suite.
Declare the primitive for a PAKE cipher suite.
Retrieve the PAKE family from a PAKE cipher suite.
Retrieve the PAKE primitive bit-size from a PAKE cipher suite.
Retrieve the hash algorithm from a PAKE cipher suite.
Declare the hash algorithm for a PAKE cipher suite.
Return an initial value for an PAKE operation object.
Set the session information for a password-authenticated key exchange.
Set the password for a password-authenticated key exchange from key ID.
Set the user ID for a password-authenticated key exchange.
Set the peer ID for a password-authenticated key exchange.
Set the application role for a password-authenticated key exchange.
Get output for a step of a password-authenticated key exchange.
Provide input for a step of a password-authenticated key exchange.
Get implicitly confirmed shared secret from a PAKE.
Abort a PAKE operation.
Macros#
A value to indicate no role in a PAKE algorithm.
The first peer in a balanced PAKE.
The second peer in a balanced PAKE.
The client in an augmented PAKE.
The server in an augmented PAKE.
The PAKE primitive type indicating the use of elliptic curves.
The PAKE primitive type indicating the use of Diffie-Hellman groups.
Construct a PAKE primitive from type, family and bit-size.
The key share being sent to or received from the peer.
A Schnorr NIZKP public key.
A Schnorr NIZKP proof.
Typedef Documentation#
psa_pake_role_t#
typedef uint8_t psa_pake_role_t
Encoding of the application role of PAKE.
Encodes the application's role in the algorithm is being executed. For more information see the documentation of individual PSA_PAKE_ROLE_XXX
constants.
914
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_step_t#
typedef uint8_t psa_pake_step_t
Encoding of input and output indicators for PAKE.
Some PAKE algorithms need to exchange more data than just a single key share. This type is for encoding additional input and output data for such algorithms.
922
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_primitive_type_t#
typedef uint8_t psa_pake_primitive_type_t
Encoding of the type of the PAKE's primitive.
Values defined by this standard will never be in the range 0x80-0xff. Vendors who define additional types must use an encoding in this range.
For more information see the documentation of individual PSA_PAKE_PRIMITIVE_TYPE_XXX
constants.
932
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_family_t#
typedef uint8_t psa_pake_family_t
Encoding of the family of the primitive associated with the PAKE.
For more information see the documentation of individual PSA_PAKE_PRIMITIVE_TYPE_XXX
constants.
939
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_primitive_t#
typedef uint32_t psa_pake_primitive_t
Encoding of the primitive associated with the PAKE.
For more information see the documentation of the PSA_PAKE_PRIMITIVE macro.
945
of file util/third_party/mbedtls/include/psa/crypto_extra.h
Function Documentation#
psa_pake_cipher_suite_init#
static struct psa_pake_cipher_suite_s psa_pake_cipher_suite_init (void)
Return an initial value for a PAKE cipher suite object.
N/A |
1836
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_get_algorithm#
static psa_algorithm_t psa_pake_cs_get_algorithm (const psa_pake_cipher_suite_t *cipher_suite)
Retrieve the PAKE algorithm from a PAKE cipher suite.
[in] | cipher_suite | The cipher suite structure to query. |
Returns
The PAKE algorithm stored in the cipher suite structure.
1767
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_set_algorithm#
static void psa_pake_cs_set_algorithm (psa_pake_cipher_suite_t *cipher_suite, psa_algorithm_t algorithm)
Declare the PAKE algorithm for the cipher suite.
[out] | cipher_suite | The cipher suite structure to write to. |
N/A | algorithm | The PAKE algorithm to write. ( |
This function overwrites any PAKE algorithm previously set in cipher_suite
.
1773
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_get_primitive#
static psa_pake_primitive_t psa_pake_cs_get_primitive (const psa_pake_cipher_suite_t *cipher_suite)
Retrieve the primitive from a PAKE cipher suite.
[in] | cipher_suite | The cipher suite structure to query. |
Returns
The primitive stored in the cipher suite structure.
1783
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_set_primitive#
static void psa_pake_cs_set_primitive (psa_pake_cipher_suite_t *cipher_suite, psa_pake_primitive_t primitive)
Declare the primitive for a PAKE cipher suite.
[out] | cipher_suite | The cipher suite structure to write to. |
N/A | primitive | The primitive to write. If this is 0, the primitive type in |
This function overwrites any primitive previously set in cipher_suite
.
1790
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_get_family#
static psa_pake_family_t psa_pake_cs_get_family (const psa_pake_cipher_suite_t *cipher_suite)
Retrieve the PAKE family from a PAKE cipher suite.
[in] | cipher_suite | The cipher suite structure to query. |
Returns
The PAKE family stored in the cipher suite structure.
1799
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_get_bits#
static uint16_t psa_pake_cs_get_bits (const psa_pake_cipher_suite_t *cipher_suite)
Retrieve the PAKE primitive bit-size from a PAKE cipher suite.
[in] | cipher_suite | The cipher suite structure to query. |
Returns
The PAKE primitive bit-size stored in the cipher suite structure.
1805
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_get_hash#
static psa_algorithm_t psa_pake_cs_get_hash (const psa_pake_cipher_suite_t *cipher_suite)
Retrieve the hash algorithm from a PAKE cipher suite.
[in] | cipher_suite | The cipher suite structure to query. |
Returns
The hash algorithm stored in the cipher suite structure. The return value is 0 if the PAKE is not parametrised by a hash algorithm or if the hash algorithm is not set.
1811
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_cs_set_hash#
static void psa_pake_cs_set_hash (psa_pake_cipher_suite_t *cipher_suite, psa_algorithm_t hash)
Declare the hash algorithm for a PAKE cipher suite.
[out] | cipher_suite | The cipher suite structure to write to. |
N/A | hash | The hash involved in the cipher suite. ( |
This function overwrites any hash algorithm previously set in cipher_suite
.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
1817
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_operation_init#
static struct psa_pake_operation_s psa_pake_operation_init (void)
Return an initial value for an PAKE operation object.
N/A |
1842
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_setup#
psa_status_t psa_pake_setup (psa_pake_operation_t *operation, const psa_pake_cipher_suite_t *cipher_suite)
Set the session information for a password-authenticated key exchange.
[inout] | operation | The operation object to set up. It must have been initialized but not set up yet. |
[in] | cipher_suite | The cipher suite to use. (A cipher suite fully characterizes a PAKE algorithm and determines the algorithm as well.) |
The sequence of operations to set up a password-authenticated key exchange is as follows:
Allocate an operation object which will be passed to all the functions listed here.
Initialize the operation object with one of the methods described in the documentation for #psa_pake_operation_t, e.g. #PSA_PAKE_OPERATION_INIT.
Call psa_pake_setup() to specify the cipher suite.
Call
psa_pake_set_xxx()
functions on the operation to complete the setup. The exact sequence ofpsa_pake_set_xxx()
functions that needs to be called depends on the algorithm in use.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
A typical sequence of calls to perform a password-authenticated key exchange:
Call psa_pake_output(operation, PSA_PAKE_STEP_KEY_SHARE, ...) to get the key share that needs to be sent to the peer.
Call psa_pake_input(operation, PSA_PAKE_STEP_KEY_SHARE, ...) to provide the key share that was received from the peer.
Depending on the algorithm additional calls to psa_pake_output() and psa_pake_input() might be necessary.
Call psa_pake_get_implicit_key() for accessing the shared secret.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
If an error occurs at any step after a call to psa_pake_setup(), the operation will need to be reset by a call to psa_pake_abort(). The application may call psa_pake_abort() at any time after the operation has been initialized.
After a successful call to psa_pake_setup(), the application must eventually terminate the operation. The following events terminate an operation:
A call to psa_pake_abort().
A successful call to psa_pake_get_implicit_key().
1308
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_set_password_key#
psa_status_t psa_pake_set_password_key (psa_pake_operation_t *operation, mbedtls_svc_key_id_t password)
Set the password for a password-authenticated key exchange from key ID.
[inout] | operation | The operation object to set the password for. It must have been set up by psa_pake_setup() and not yet in use (neither psa_pake_output() nor psa_pake_input() has been called yet). It must be on operation for which the password hasn't been set yet (psa_pake_set_password_key() hasn't been called yet). |
N/A | password | Identifier of the key holding the password or a value derived from the password (eg. by a memory-hard function). It must remain valid until the operation terminates. It must be of type PSA_KEY_TYPE_PASSWORD or PSA_KEY_TYPE_PASSWORD_HASH. It has to allow the usage PSA_KEY_USAGE_DERIVE. |
Call this function when the password, or a value derived from the password, is already present in the key store.
1356
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_set_user#
psa_status_t psa_pake_set_user (psa_pake_operation_t *operation, const uint8_t *user_id, size_t user_id_len)
Set the user ID for a password-authenticated key exchange.
[inout] | operation | The operation object to set the user ID for. It must have been set up by psa_pake_setup() and not yet in use (neither psa_pake_output() nor psa_pake_input() has been called yet). It must be on operation for which the user ID hasn't been set (psa_pake_set_user() hasn't been called yet). |
[in] | user_id | The user ID to authenticate with. |
N/A | user_id_len | Size of the |
Call this function to set the user ID. For PAKE algorithms that associate a user identifier with each side of the session you need to call psa_pake_set_peer() as well. For PAKE algorithms that associate a single user identifier with the session, call psa_pake_set_user() only.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
1396
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_set_peer#
psa_status_t psa_pake_set_peer (psa_pake_operation_t *operation, const uint8_t *peer_id, size_t peer_id_len)
Set the peer ID for a password-authenticated key exchange.
[inout] | operation | The operation object to set the peer ID for. It must have been set up by psa_pake_setup() and not yet in use (neither psa_pake_output() nor psa_pake_input() has been called yet). It must be on operation for which the peer ID hasn't been set (psa_pake_set_peer() hasn't been called yet). |
[in] | peer_id | The peer's ID to authenticate. |
N/A | peer_id_len | Size of the |
Call this function in addition to psa_pake_set_user() for PAKE algorithms that associate a user identifier with each side of the session. For PAKE algorithms that associate a single user identifier with the session, call psa_pake_set_user() only.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
1438
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_set_role#
psa_status_t psa_pake_set_role (psa_pake_operation_t *operation, psa_pake_role_t role)
Set the application role for a password-authenticated key exchange.
[inout] | operation | The operation object to specify the application's role for. It must have been set up by psa_pake_setup() and not yet in use (neither psa_pake_output() nor psa_pake_input() has been called yet). It must be on operation for which the application's role hasn't been specified (psa_pake_set_role() hasn't been called yet). |
N/A | role | A value of type psa_pake_role_t indicating the application's role in the PAKE the algorithm that is being set up. For more information see the documentation of |
Not all PAKE algorithms need to differentiate the communicating entities. It is optional to call this function for PAKEs that don't require a role to be specified. For such PAKEs the application role parameter is ignored, or PSA_PAKE_ROLE_NONE can be passed as role
.
Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
1480
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_output#
psa_status_t psa_pake_output (psa_pake_operation_t *operation, psa_pake_step_t step, uint8_t *output, size_t output_size, size_t *output_length)
Get output for a step of a password-authenticated key exchange.
[inout] | operation | Active PAKE operation. |
N/A | step | The step of the algorithm for which the output is requested. |
[out] | output | Buffer where the output is to be written in the format appropriate for this |
N/A | output_size | Size of the |
[out] | output_length | On success, the number of bytes of the returned output. |
Depending on the algorithm being executed, you might need to call this function several times or you might not need to call this at all.
The exact sequence of calls to perform a password-authenticated key exchange depends on the algorithm in use. Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_pake_abort().
1538
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_input#
psa_status_t psa_pake_input (psa_pake_operation_t *operation, psa_pake_step_t step, const uint8_t *input, size_t input_length)
Provide input for a step of a password-authenticated key exchange.
[inout] | operation | Active PAKE operation. |
N/A | step | The step for which the input is provided. |
[in] | input | Buffer containing the input in the format appropriate for this |
N/A | input_length | Size of the |
Depending on the algorithm being executed, you might need to call this function several times or you might not need to call this at all.
The exact sequence of calls to perform a password-authenticated key exchange depends on the algorithm in use. Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
If this function returns an error status, the operation enters an error state and must be aborted by calling psa_pake_abort().
1593
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_get_implicit_key#
psa_status_t psa_pake_get_implicit_key (psa_pake_operation_t *operation, psa_key_derivation_operation_t *output)
Get implicitly confirmed shared secret from a PAKE.
[inout] | operation | Active PAKE operation. |
[out] | output | A key derivation operation that is ready for an input step of type PSA_KEY_DERIVATION_INPUT_SECRET. |
At this point there is a cryptographic guarantee that only the authenticated party who used the same password is able to compute the key. But there is no guarantee that the peer is the party it claims to be and was able to do so.
That is, the authentication is only implicit. Since the peer is not authenticated yet, no action should be taken yet that assumes that the peer is who it claims to be. For example, do not access restricted files on the peer's behalf until an explicit authentication has succeeded.
This function can be called after the key exchange phase of the operation has completed. It imports the shared secret output of the PAKE into the provided derivation operation. The input step PSA_KEY_DERIVATION_INPUT_SECRET is used when placing the shared key material in the key derivation operation.
The exact sequence of calls to perform a password-authenticated key exchange depends on the algorithm in use. Refer to the documentation of individual PAKE algorithm types (PSA_ALG_XXX
values of type psa_algorithm_t such that PSA_ALG_IS_PAKE(alg
) is true) for more information.
When this function returns successfully, operation
becomes inactive. If this function returns an error status, both operation
and key_derivation
operations enter an error state and must be aborted by calling psa_pake_abort() and psa_key_derivation_abort() respectively.
1656
of file util/third_party/mbedtls/include/psa/crypto_extra.h
psa_pake_abort#
psa_status_t psa_pake_abort (psa_pake_operation_t *operation)
Abort a PAKE operation.
[inout] | operation | The operation to abort. |
Aborting an operation frees all associated resources except for the operation
structure itself. Once aborted, the operation object can be reused for another operation by calling psa_pake_setup() again.
This function may be called at any time after the operation object has been initialized as described in #psa_pake_operation_t.
In particular, calling psa_pake_abort() after the operation has been terminated by a call to psa_pake_abort() or psa_pake_get_implicit_key() is safe and has no effect.
1683
of file util/third_party/mbedtls/include/psa/crypto_extra.h
Macro Definition Documentation#
PSA_PAKE_ROLE_NONE#
#define PSA_PAKE_ROLE_NONEValue:
((psa_pake_role_t)0x00)
A value to indicate no role in a PAKE algorithm.
This value can be used in a call to psa_pake_set_role() for symmetric PAKE algorithms which do not assign roles.
951
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_ROLE_FIRST#
#define PSA_PAKE_ROLE_FIRSTValue:
((psa_pake_role_t)0x01)
The first peer in a balanced PAKE.
Although balanced PAKE algorithms are symmetric, some of them needs an ordering of peers for the transcript calculations. If the algorithm does not need this, both PSA_PAKE_ROLE_FIRST and PSA_PAKE_ROLE_SECOND are accepted.
960
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_ROLE_SECOND#
#define PSA_PAKE_ROLE_SECONDValue:
((psa_pake_role_t)0x02)
The second peer in a balanced PAKE.
Although balanced PAKE algorithms are symmetric, some of them needs an ordering of peers for the transcript calculations. If the algorithm does not need this, either PSA_PAKE_ROLE_FIRST or PSA_PAKE_ROLE_SECOND are accepted.
969
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_ROLE_CLIENT#
#define PSA_PAKE_ROLE_CLIENTValue:
((psa_pake_role_t)0x11)
The client in an augmented PAKE.
Augmented PAKE algorithms need to differentiate between client and server.
975
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_ROLE_SERVER#
#define PSA_PAKE_ROLE_SERVERValue:
((psa_pake_role_t)0x12)
The server in an augmented PAKE.
Augmented PAKE algorithms need to differentiate between client and server.
981
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_PRIMITIVE_TYPE_ECC#
#define PSA_PAKE_PRIMITIVE_TYPE_ECCValue:
((psa_pake_primitive_type_t)0x01)
The PAKE primitive type indicating the use of elliptic curves.
The values of the family
and bits
fields of the cipher suite identify a specific elliptic curve, using the same mapping that is used for ECC (psa_ecc_family_t) keys.
(Here family
means the value returned by psa_pake_cs_get_family() and bits
means the value returned by psa_pake_cs_get_bits().)
Input and output during the operation can involve group elements and scalar values:
The format for group elements is the same as for public keys on the specific curve would be. For more information, consult the documentation of psa_export_public_key().
The format for scalars is the same as for private keys on the specific curve would be. For more information, consult the documentation of psa_export_key().
1001
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_PRIMITIVE_TYPE_DH#
#define PSA_PAKE_PRIMITIVE_TYPE_DHValue:
((psa_pake_primitive_type_t)0x02)
The PAKE primitive type indicating the use of Diffie-Hellman groups.
The values of the family
and bits
fields of the cipher suite identify a specific Diffie-Hellman group, using the same mapping that is used for Diffie-Hellman (psa_dh_family_t) keys.
(Here family
means the value returned by psa_pake_cs_get_family() and bits
means the value returned by psa_pake_cs_get_bits().)
Input and output during the operation can involve group elements and scalar values:
The format for group elements is the same as for public keys on the specific group would be. For more information, consult the documentation of psa_export_public_key().
The format for scalars is the same as for private keys on the specific group would be. For more information, consult the documentation of psa_export_key().
1021
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_PRIMITIVE#
#define PSA_PAKE_PRIMITIVEValue:
Construct a PAKE primitive from type, family and bit-size.
Returns
The constructed primitive value of type psa_pake_primitive_t. Return 0 if the requested primitive can't be encoded as psa_pake_primitive_t.
1042
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_STEP_KEY_SHARE
#define PSA_PAKE_STEP_KEY_SHAREValue:
((psa_pake_step_t)0x01)
The key share being sent to or received from the peer.
The format for both input and output at this step is the same as for public keys on the group determined by the primitive (psa_pake_primitive_t) would be.
For more information on the format, consult the documentation of psa_export_public_key().
For information regarding how the group is determined, consult the documentation PSA_PAKE_PRIMITIVE.
1059
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_STEP_ZK_PUBLIC#
#define PSA_PAKE_STEP_ZK_PUBLICValue:
((psa_pake_step_t)0x02)
A Schnorr NIZKP public key.
This is the ephemeral public key in the Schnorr Non-Interactive Zero-Knowledge Proof (the value denoted by the letter 'V' in RFC 8235).
The format for both input and output at this step is the same as for public keys on the group determined by the primitive (psa_pake_primitive_t) would be.
For more information on the format, consult the documentation of psa_export_public_key().
For information regarding how the group is determined, consult the documentation PSA_PAKE_PRIMITIVE.
1076
of file util/third_party/mbedtls/include/psa/crypto_extra.h
PSA_PAKE_STEP_ZK_PROOF#
#define PSA_PAKE_STEP_ZK_PROOFValue:
((psa_pake_step_t)0x03)
A Schnorr NIZKP proof.
This is the proof in the Schnorr Non-Interactive Zero-Knowledge Proof (the value denoted by the letter 'r' in RFC 8235).
Both for input and output, the value at this step is an integer less than the order of the group selected in the cipher suite. The format depends on the group as well:
For Montgomery curves, the encoding is little endian.
For everything else the encoding is big endian (see Section 2.3.8 of SEC 1: Elliptic Curve Cryptography at https://www.secg.org/sec1-v2.pdf).
In both cases leading zeroes are allowed as long as the length in bytes does not exceed the byte length of the group order.
For information regarding how the group is determined, consult the documentation PSA_PAKE_PRIMITIVE.
1097
of file util/third_party/mbedtls/include/psa/crypto_extra.h