A version structure containing all version information.

Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

build#

uint16_t EmberVersion::build

Definition at line 97 of file ./stack/include/ember-types.h

major#

uint8_t EmberVersion::major

Definition at line 98 of file ./stack/include/ember-types.h

minor#

uint8_t EmberVersion::minor

Definition at line 99 of file ./stack/include/ember-types.h

patch#

uint8_t EmberVersion::patch

Definition at line 100 of file ./stack/include/ember-types.h

special#

uint8_t EmberVersion::special

Definition at line 101 of file ./stack/include/ember-types.h

type#

EmberVersionType EmberVersion::type

Definition at line 102 of file ./stack/include/ember-types.h