Defines a ZigBee network and the associated parameters.

Public Attributes#

uint16_t
uint8_t

Public Attribute Documentation#

panId#

uint16_t EmberZigbeeNetwork::panId

Definition at line 576 of file ./stack/include/ember-types.h

channel#

uint8_t EmberZigbeeNetwork::channel

Definition at line 577 of file ./stack/include/ember-types.h

allowingJoin#

bool EmberZigbeeNetwork::allowingJoin

Definition at line 578 of file ./stack/include/ember-types.h

extendedPanId#

uint8_t EmberZigbeeNetwork::extendedPanId[EXTENDED_PAN_ID_SIZE]

Definition at line 579 of file ./stack/include/ember-types.h

stackProfile#

uint8_t EmberZigbeeNetwork::stackProfile

Definition at line 580 of file ./stack/include/ember-types.h

nwkUpdateId#

uint8_t EmberZigbeeNetwork::nwkUpdateId

Definition at line 581 of file ./stack/include/ember-types.h