Struct wrapper for all data for a command which comes in over the air. This enables struct is used to encapsulate a command in a single place on the stack and pass a pointer to that location around during command processing.
Public Attribute Documentation#
apsFrame#
EmberApsFrame* EmberAfClusterCommand::apsFrame
APS frame for the incoming message
type#
EmberIncomingMessageType EmberAfClusterCommand::type
source#
EmberNodeId EmberAfClusterCommand::source
buffer#
uint8_t* EmberAfClusterCommand::buffer
bufLen#
uint16_t EmberAfClusterCommand::bufLen
clusterSpecific#
bool EmberAfClusterCommand::clusterSpecific
mfgSpecific#
bool EmberAfClusterCommand::mfgSpecific
mfgCode#
uint16_t EmberAfClusterCommand::mfgCode
seqNum#
uint8_t EmberAfClusterCommand::seqNum
commandId#
uint8_t EmberAfClusterCommand::commandId
payloadStartIndex#
uint8_t EmberAfClusterCommand::payloadStartIndex
direction#
uint8_t EmberAfClusterCommand::direction
interPanHeader
EmberAfInterpanHeader* EmberAfClusterCommand::interPanHeader
networkIndex#
uint8_t EmberAfClusterCommand::networkIndex