Use for the information retrieved during a response to an Ember Bootloader over-the-air query.
Public Attribute Documentation#
hardwareTag#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::hardwareTag[EMBER_AF_STANDALONE_BOOTLOADER_HARDWARE_TAG_LENGTH]
eui64#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::eui64[EUI64_SIZE]
mfgId#
uint16_t EmberAfStandaloneBootloaderQueryResponseData::mfgId
bootloaderVersion#
uint16_t EmberAfStandaloneBootloaderQueryResponseData::bootloaderVersion
capabilities#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::capabilities
platform#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::platform
micro#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::micro
phy#
uint8_t EmberAfStandaloneBootloaderQueryResponseData::phy
bootloaderActive#
bool EmberAfStandaloneBootloaderQueryResponseData::bootloaderActive